|
Discover OpenScape UC Server, the open software foundation for Unified Communications solutions.
Open Minds
Regístrese en Open Minds y recibirá la última información sobre Open Communications directamente en su bandeja de correo.
Alta
+34 900 100 566

OpenScape Unified Communications (UC) Server

An ingenious approach to communication

Siemens has launched an innovative new unified communications software platform; the OpenScape Unified Communications (UC) Server.  The OpenScape UC Server is a revolution in communication design. It removes the artificial legacy barriers between today’s traditionally separate voice, video and unified communications systems to support a comprehensive suite of UC applications. This suite will initially include enterprise grade voice with carrier grade scalability and reliability, IP least cost routing, video conferencing and role-based UC applications.  

OpenScape UC Server software is the foundation for the new OpenScape Unified Communications Suite.  The OpenScape UC Server enables presence, administration, session control and other shared services across the current family of OpenScape UC Suite of applications.

What’s in it for my business?

Unification of communications into this comprehensive suite represents a key strategic step to improving customer response and enterprise agility. On-demand access to people and information accelerates decision making, reduces process latency and encourages collaboration and the effective exchange of ideas. Flexible working increases productivity.

This ingenious piece of kit is easy to integrate into your business, as OpenScape UC Server can operate in any existing IT or telephony environment. This includes IP telephony or legacy PBX telephony environments from Siemens or any other vendor.  Installation is simple and affordable, with practical options that don’t require expensive or complex proprietary technology stacks.

Grow modularly when you need to

The design of the OpenScape UC Server software enables easy growth and expansion in line with the growth of your business when appropriate. New modular capabilities can be set up simply by activating the desired license keys on a user-by-user basis.  The family of OpenScape UC Suite of applications will expand in the future.

In accordance with Siemens’ Open Communications approach, OpenScape UC Server has been built from the ground up as an open, SIP-based, software IT communications and UC application foundation with shared web-services components that leverage Siemens’ OpenSOA architecture.  

No need to change equipment

Using HiPath 8000 and HiPath OpenExchange already? These applications have been redesigned to run natively on the OpenScape UC Server for enterprise voice and IP least cost routing.  All of the OpenScape UC suite of applications slot easily into whatever systems you use currently. They operate in multi-vendor environments and integrate with complementary offerings including IBM Sametime and Microsoft Office Communication Server.

The OpenScape UC Server is appropriate for any organization with 1000 users or more and will be available in three versions.  The Medium Edition (ME) configuration is a single server solution with optional redundancy for up to 1,000 users. Large enterprise? The Large Edition (LE) is a multi-server configuration for up to 100,000 users. Up to 20,000 of those receive full UC functionality and up to 100,000 basic UC functionality.  The Hosted Edition (HE) contains additional application components to support the unique requirements of service providers and hosting organisations.  

“With the introduction of OpenScape Unified Communications Server, we have reached a significant milestone in our transition from a traditional VoIP manufacturer to a top global software and services company focused on a new era in the enterprise communications market. Simply put, OpenScape UC Server is the easiest, most affordable and flexible way to introduce full UC into any existing telephony or IT environment.”
Eve Aretakis, CEO, Siemens Communications, Inc.  

Contact us
Find out more about how the OpenScape UC Suite of applications could benefit your business.