Bada Bing
All the latest stuff on Open Communications ready to download. Sorted.
Open Minds
Register for the latest information.
Register for Open Minds
+44 (0)20 7526 4861 (UK)/ +353 (0)1 216 2000 (IRE)
RSS

OpenScape Contact Center Offers Enhanced Multi-Tenancy Capabilities

Munich, Dec 16, 2008

Siemens OpenScape® Contact Center Offers Enhanced Multi-Tenancy Capabilities in an Easy-to-Own, Easy-to-Deploy Acquisition Model

Release Also Provides Virtualized Contact Center Capabilities in Scalable, Pre-packaged Software Modules, So Companies Can More Easily and More Affordably Add Functionality As Needs Change

Siemens announced today the latest release of its OpenScape Contact Center, a highly scalable, virtualized contact center software platform. It is now available via a multi-tenancy license, which is acquired just once for the enterprise or managed services provider so business units or subscribers can then be added more easily upon request. In addition, pre-packaged modules offer customers the chance to add functionality on the same platform whenever needed. This acquisition model is designed to provide a simpler and more affordable way to deploy virtualized contact center capabilities, while leveraging existing investments and skill sets.

 

The Siemens OpenScape Contact Center solution can be hosted as a secure multi-tenant platform in a data center on just one enterprise or managed services server. With secure server partitioning, its many capabilities and services can be widely distributed among “local tenants.” These are the various enterprise business units or managed service provider subscribers, which may operate from any number of different locations and have their virtualized contact center features completely and securely localized for their needs.

 

With enhanced multi-tenancy capabilities, operators can avoid the geographic limitations and inherent inefficiencies of having many siloed, site-based installations. Specifically, enhancements to the Siemens OpenScape Contact Center solution include:

•     Massive scalability, with up to 1,500 active agents supported by a single server, across multiple business entities, each one with separate administration and security; design and routing; and monitoring and reporting

•     Support for multiple time zones for deployments having geographically separate entities

•     A manager desktop that provides business-level permissions and system access

•     Enhanced security for improved manager/supervisor productivity within each business entity

One platform, one deploymentThe OpenScape Contact Center can be deployed over virtually any existing communications or IT network infrastructure, requiring fewer IT and administration resources for support. Sharing virtualized contact center resources this way helps to minimize capital investment, while helping to maximize operational efficiency when compared to managing multiple incompatible vendor contact center platforms. The centralized approach significantly simplifies contact center management.

 

According to Joe Outlaw, principal contact center analyst for Frost and Sullivan, “Multi-tenant contact center applications are not new, but what is significant in this release of the Siemens OpenScape Contact Center is the level of sophisticated multi-tenant capabilities in an easy to acquire, configure and administer form factor. I expect this reduced complexity and the related cost advantages will be attractive to customers and service providers considering multi-tenant solutions.”

Localized operation for each local tenantThe Siemens OpenScape Contact Center solution provides self-administration capabilities to each local tenant. It is also designed to ensure that local supervisors can control only those administrative functions, user views, reporting, routing and queue control for which they are responsible. New multiple time zone features further localize the agent and administrative functions with center-specific reports and wallboard displays. The new automated reporting facility distributed by email provides operational support regardless of the manager’s physical location.

Enhanced security and data retentionThe Siemens OpenScape Contact Center solution comes with enhanced security tools. Super-manager hierarchy is designed to ensure that user-based permission is required for administration, routing, monitoring, reporting and data storage functions. While this can improve permission-based supervisor roles, it can also provide greater peace of mind for customers in regulated industries, such as healthcare and financial services, that require options for tighter control and security of transactions.

 

“The Siemens OpenScape Contact Center solution provides a centrally managed virtual business model for enterprises and managed service providers alike that seek to optimize their allocation of both agent and system resources, while minimizing total cost of ownership,” said Ross Sedgewick, Director Global Marketing Large Enterprise Solutions. “What’s more, our acquisition model enables companies and service providers an easier and more affordable way to license and share the rich functionality of the Siemens OpenScape Contact Center platform while adding functionality as they grow or their needs change.”

 

The Siemens OpenScape Contact Center solution will be available in February 2009, through all channels. System list pricing for new multi-tenancy software options start at 3.250 Euro.