Bada Bing
All the latest stuff on Open Communications ready to download. Sorted.
Latest Articles for February 2007
26 February 2007
Siemens Enterprise Communications today launched HiPath MobileConnect, an enterprise FMC solution that seamlessly unifies fixed enterprise VoIP, VoWLAN and cellular networks, which will also be one of Siemens' highlights at CeBIT in Hannover, presented at booth D 37 in hall 13. The result for businesses is an increase in productivity and responsiveness while driving mobile call communications costs down. MobileConnect is the only end-to-end solution that delivers one number and one mailbox with a seamless handover between wireless (WiFi) and cellular networks delivered on a single device.